2017-08-04 6:32 AM
Hi everyone,
I have a weird problem with the powerstep01 on a X-NUCLEO-IHM03A1. I want to change to driver parameters KVAL_HOLD, KVAL_RUN, KVAL_ACC, KVAL_DEC, INT_SPEED, ST_SLP, FN_SLP_ACC, FN_SLP_DEC. All works as expected as long as I use a single board. However, if I use use a stack of three boards in a daisy chain I can only change
KVAL_
HOLD
, KVAL_RUN, KVAL_ACC, KVAL_DEC while the other parameters remain unchanged. All motors are stopped and HiZ.
Any help is much appreciated.
#powerstep01-stepper-motor-driver #powerstep01Solved! Go to Solution.
2017-08-04 7:55 AM
Ok, I got it. Issued a soft stop command before writing to the registers which forces the motors out of HiZ. Use of the soft_hiz command fixed the issue.
2017-08-04 7:55 AM
Ok, I got it. Issued a soft stop command before writing to the registers which forces the motors out of HiZ. Use of the soft_hiz command fixed the issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.