2020-04-09 6:44 PM
I need to run a while LED (output voltage range from 2.5-4.5v 4A surge, 3A steady state) from a battery source that can range from 3v to 6.4v in. So it's a buck-boost. I haven't been able to find a buck-boost that has a Vin higher than 5, with an absolute max of 5.5. The 6.4v is going to drop under load but it will still be above 5.5. I was wondering if I should just put a load resistor in series and bypass it when the Vin drops enough. Does anyone have any suggestions?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.