2025-01-30 9:00 AM - last edited on 2025-01-31 12:35 AM by Peter BENSCH
Hello,
I have questions about a project we developed a long time ago. I will put the schematic below. We are using the BTA26-800BWRG (U8 and U9) in the schematic to parallel two inductors. The voltage applied to these two inductors is an ultrasonic signal of 600V at a frequency of 20-120 kHz. However, I don't fully understand how the TRIACs can switch, given that there is no voltage source in the loop between the two gates. Yet, the project works almost perfectly, except that sometimes, when the generator is off and the attempt is made to turn off the TRIACs, they remain switched on.
U8 & U9 (BTA26-800BWRG) & OP1 & OP2 (IL410)
Thank's in advance for your help.
Best regards,
Joe
2025-02-03 12:45 AM
An ultrasonic generator is connected to the J200 & J201. The triacs are there just for changing the value of the inductance (in parallel). In fact we generate a square wave from 400VDC. Then we use the principe of resonance with Inductance / Ultrasonic transducer (Which is electrically like a capacitor). The square wave as a frequency between 20-120 kHz wich depend of the transducer mounted. The triacs is used when we have bifrequency transducer to permute. We change the frequency and we have also to change the value of the inductance to have a resonant system... Hope it's now more clear
2025-02-03 2:17 AM
The community is a worldwide forum for mutual help between users of devices from STMicroelectronics. As I have already mentioned, you cannot assume that all users are familiar with the basic functioning of your system. I also see an ultrasonic generator as a device to which a transducer will be connected. However, if your system already has a transducer, you should explain where exactly your two points J200 and J201 are connected: parallel to the transducer?
In addition, I still don't understand what the problem is when the generator is switched off. When it is switched off, there should be no voltage at the terminals?
2025-02-03 3:03 AM
Yes the transducer is connected parallel with the inductance. An ultrasonic generator is just an electrical generator.
As I have mention the generator provide a square wave from 400VDC and the frequency is between 20 and 120 kHZ.
When the generator is switched off there is no more power applied on the J200/J201.
I'm really sorry if my explanation aren't enough clear...
2025-02-03 5:10 AM
Your explanations still don't give a clear picture. Such ping-pong questions to finally understand what the problem actually is will not help you or future readers of this forum. You have mentioned several times that the triacs are not switched off:
Post 1: "sometimes, when the generator is off and the attempt is made to turn off the TRIACs, they remain switched on."
Post 2: "I just have no idea how to correct the little bug with the switch off."
Post 3: The Triacs still passing even if the self_commut signal is at 0. Most of case when we turn off the generator, try to switch off the TRIAC, and then turn back on.
Post 4: The problem occurs only when the generator is turned off... I wonder if the inductance does not add a DC voltage to the system at the moment the generator is turned off.
Post 6: When the generator is switched off there is no more power applied on the J200/J201.
If a generator is switched off, it supplies no longer energy to its terminals. How do you know that the triacs are still switched on when there is no longer any voltage across their terminals and therefore no current anymore?
2025-02-03 6:03 AM - edited 2025-02-03 6:25 AM
Don't know what is still not clear for you...?
Generator (Square wave 400V --> 20-120 kHz) connected to:
1. Inductance 1
2. Inductance 2
3. Ultrasonic transducer
Triacs are used to connect or not the inductance 2 (to the generator)
Then I try to switch off the triacs, turn back on the generator, then I see that the triacs are still switched... (Inductrance In parallel --> I have the good inductance --> the resonance is good --> more power consumed)
When I do same operation with generator turned on I have no problem.
2025-02-03 6:34 AM
However, excited resonant circuits usually have a very high voltage due to the resonance, so that triacs can be triggered even without external control via their gates. This is probably why you can separate your coils more cleanly with a suitable relay than with antiserial triacs.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.