Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Controlling L6470 Using SPI

Posted on November 09, 2014 at 21:23Hello, I'm having a lot of trouble trying to simply talk to the L6470 using SPI. When I send any byte whether it be a valid command or not, the L6470 simply sends the command back on the next SPI transfer. How is ...

wil by Associate
  • 893 Views
  • 1 replies
  • 0 kudos

L6480: Power & Comm problem

Posted on August 21, 2014 at 16:45I'm currently experiencing a problem in which I cannot get the L6480 device to communicate - I think this may be due to a device power up fault but I was hoping someone on here could help!I've attached a simplified ...

hj_smith by Associate
  • 2278 Views
  • 3 replies
  • 0 kudos

Communication via SPI with L6470 in mode daisy chain

Posted on October 09, 2012 at 10:45Hello I'm trying to communicate with SPI from my application in C with two L6470 configured in daisy chain mode. Sending data but I get no response from the pin DSO of  the first L6470. Someone can tell me the step...

jartigas by Associate II
  • 3030 Views
  • 8 replies
  • 0 kudos

L6561/L6562 MathCad design tool

Posted on October 30, 2014 at 22:06The document AN1089 CONTROL LOOP MODELING OF L6561-BASED TM PFC by Claudio Adragna says: ''As a tool to ease the design of L6561�s E/A compensation networks in TM boost PFC preregulators, the Appendix contains a Ma...

jbright by Associate II
  • 1254 Views
  • 1 replies
  • 0 kudos

L6229Q EN internally connected to DIAG

Posted on October 21, 2014 at 00:52In the datasheet for the L6229Q, section 5.2 states ''Pin EN (Enable) has identical input structure with the exception that the drain of the overcurrent and thermal protection MOSFET is also connected to this pin.'...

jcarlson by Associate
  • 928 Views
  • 1 replies
  • 0 kudos

No working devices issue.

Posted on October 17, 2014 at 05:56 Hello, I see this question in the forum, but no one reply. Can anyone help to feedback how to solve this problem? Because I encountered this issue too. Thanks. ===========================================...

0690X0000060MoWQAU.gif

Motor electrical parameters

Posted on October 24, 2014 at 14:53Hi, I am not entierly sure how to correctly enter my motor parameters, and which effect they have, can anyone check if I am doing this correctly (sensorless operation with cordic startup, no extra features like flu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.