Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

need whitepaper!

i could not receive whitepaper which is titled "How to save space and eliminate unnecessary cabling in space-constrained vehicles" even i filled out the form...please give me support. Whitepaper: How to save space and eliminate unnecessary cabling in...

ro1 by Associate II
  • 541 Views
  • 0 replies
  • 0 kudos

L9963E addressing issue.

I having issue addressing L9963E when the device is already awake. Currently my team is working on developing a BMS using two L9963E in a daisy chain configuration. In some instances, we may have to reset our micro controller(eg: Soft Reset, WDT rese...

AKann.3 by Associate
  • 2028 Views
  • 2 replies
  • 0 kudos

How can I set OV UV threshold of L9963E?

 Hello, I'm trying to set UV OV value of my L9963E. I'm aware that writing "threshVcellOV" and "threshVcellUV" fields in "VCELL_THRESH_UV_OV" register to do that. However, there is no information about which bit values corresponding voltage values. A...

berg0v1c_1-1749630723134.png berg0v1c_0-1749630682714.png
berg0v1c by Associate II
  • 492 Views
  • 0 replies
  • 1 kudos

STWBC2-HP

我需要一份STWBC2-HP的原理图文件,我已经登陆了,但是我在下载的时候依旧提示我登录我还想问STWBC2-HP这个IC需不需要驱动文件,如果需要的,麻烦一并发给我谢谢。  

Fengji_0-1737596998899.png Fengji_1-1737597026024.png
Fengji by Associate II
  • 1634 Views
  • 3 replies
  • 0 kudos

STWBC2-HP Evalobard

Hi All,I have developed my own Evalboard for the STWBC2-HP based on the STEVAL-WBC2TX50. Now i have flashed the stdes-50w2cwbc_FW_v1.0.0.0.hex firmware to the board and the Software shows the following. The power transfer does not work. Do you have a...

simonh_0-1724138049367.png
simonh by Associate III
  • 3944 Views
  • 5 replies
  • 0 kudos

Designing High PF AC-DC conveter

We were designing 24v 1.5 Amp smps using l6562 referring application note AN1059 fig 16. getting the 24 output but fluctuating when load is connected and without load power factor is 1.00 and with load it drops down to 0.2 PF and which configuration ...

20250606_100505.jpg 20250606_114828.jpg 20250606_114840.jpg 20250606_114847.jpg
D_N by Associate II
  • 418 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.