Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STSPIN32F0 serial bootloader

Posted on May 16, 2017 at 12:35Hello.   I'm using an STSPIN32F0 for PMSM motor driving. Is there a way to use the serial bootloader inside the chip?

dany2 by Associate
  • 1011 Views
  • 1 replies
  • 0 kudos

FGL60N100BNTD vs. STGW40H120DF2

Posted on May 17, 2017 at 09:50I found a replacement for FGL60N100BNTD (TO-264) which is STGW40H120DF2 (TO-247) for my Inverter. At 50A peak current, however its a problem. Any reason or solution?

Properties of transils

Posted on May 16, 2017 at 07:58Hello!I need information about values of the rms current which don't result in the open-circuiting of a transil diodes type SM6T and 1.5KE and about values of I2t  for these devices.I need this informations to determin...

L9823 as Input?

Posted on April 24, 2017 at 13:15I am using L9823 in my design to drive the outputs. I also want it to behave as input so that I can connect IO module. How can I use it as input?Thanks in advance

Transils

Posted on May 15, 2017 at 12:49Hello!I need information about values of the rms current which don't result in the open-circuiting of a transil diodes type SM6T and 1.5KE and about values of I2t  for these devices.I need this informations to determin...

SPINFamily Evaluation Software - BEMF Calculation

Posted on April 18, 2017 at 14:07Hi,When I am using the BEMF compensation configuration within the SPINFamily Evaluation Software, I input the Application Parameters and the Motor Parameters for my particular motor. When I press the �Evaluate� butto...

0690X00000606nmQAA.png 0690X00000606nnQAA.png

community.st.com

Posted on May 08, 2017 at 17:03Why does my BLDC motor stop during acceleration 2 ? Hello,I bought a STSPIN32F0 and i try to run this board with a BLDC Motor. But the first 3-4 seconds is working then stops. The same problem with me onhttps://communi...

powerstep01

Posted on May 07, 2017 at 12:50An arm cortex-M0 MCU is adopted to drive the powetstep01.The initialization of SPI is done including CS, SDO, SDI, CK,BUSY, STBY.Here is the problem, I want the step motor run, so I write this:CS=low;//chip selectSPI1_...

Lin SS by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos

Viper26LN with output at 3.3v

Posted on May 04, 2017 at 18:20Hi,We are working in a project using Viper26ln to generate a 3.3V (250 mA maximum current) from an AC 220 line using buck topology because we want our circuit as compact as possible, so we  avoid using transformers.We ...

0690X00000606wPQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.