Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cooling of L6201PS Motor Driver

I want to use the L6201PS Motor Driver for a motor (24-48V) and the max. current is 4A. My Question is at which current value do I need a coolant? I found out in the datasheet that I only need some ground area for cooling, is that correct?

MS123 by Associate
  • 704 Views
  • 0 replies
  • 0 kudos

How to get STSW-L9907-H , a GUI for EVAL-L9907-H?

Can someone tell me how to download / where to find the GUI (STSW-L9907-H) for the evaluation board EVAL-L9907-H?A user manual (UM2119) is available, but the software itself is missing from the repository. STSW-L9907-H: https://my.st.com/content/my_s...

vmekr by Associate II
  • 915 Views
  • 0 replies
  • 0 kudos

X-NUCLEO-IHM15A1 for motor having 5A stall current at 12V

Hi everyone, since i'm new to motor control i have a beginner (i think) question. I'm looking for an expansion and nucleo board for my brush DC Motor(BDC). For expansion i find X-NUCLEO-IHM15A1 but it can power 1.5A for each motor. My motor has a sta...

N ORhan by Associate III
  • 1180 Views
  • 3 replies
  • 0 kudos

Do you have any advice which voltage regulator should I use?

Hi to All,I want to make a pcb card which which work with 3.6V. I wil use a voltage regulator to drop down voltage from 10V-17V batteries to 3.3V. Do you have any advice which voltage regulator should I use. I am trying to make a system with lowest p...

sahma.18 by Associate II
  • 2452 Views
  • 6 replies
  • 0 kudos

Doubts SPV1020, power optimizer

Hello, I am studying DC-DC converters, power optimizers for grid-connected PV.I saw some work with the SPV1020, but it seems to be discontinued. Do you know why? Is there a new version?I would also be grateful if I indicated any evaluation module, th...

Is there a way to default the STSpin840 motor driver to completely shut down the motor from turning upon power up?

I am currently using the X-NUCLEO-IHM15A1 Shield with the NUCLEO_F401RE MCU board to evaluate the use of the STSpin840 Motor driver using a single 12VDC motor. During the programming and debug process the motor will automatically start turning. Beca...

What do I connect pin 2 (VREFB) of the STSPIN840 to when I want to run the two outputs in parallel for higher current capability?

I am currently designing a PCB that will control a single motor using the STSPIN840 (X-NUCLEO-IHM15A1 Shield). The datasheet is pretty good about explaining how to connect things if you want to run the outputs in parallel mode but it neglets to tell...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.