Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Cost-efficient remote reset of STPM3x

STPM32 is used for an e-meter application. Idea is to use 2-pin UART connection, isolate only the RX and TX with optocouplers and not to use the SYN and SCS for reset.According to datasheet on page 68 the remote reset can be performed in two ways:·  ...

0690X00000895RgQAI.png

Resolved! Stop LED flickering with a Snubberless™ Triac

I have a problem with triac BTA06-600B, when I try to power off some LED lamps they start flickering. I use triac to manage the main power (220V 50Hz), if the load is a traditional, halogen or cfl lamp all works fine. I tried to unmount the snubber c...

0690X00000895IFQAY.png

push pull converter design

I made a push-pull converter using sg3525a. my problem is the output voltage will drop when I connecting 100-watt load or more.input voltage is 24 volt and the output is 350 volt. the frequency is 100khz. using MOSFET irfp4568. using RC snubber with ...

mrk by Associate
  • 1032 Views
  • 0 replies
  • 0 kudos

L6470 motor stalls around 1500 steps/s

Hi All!Doing a project where I need the L6470 to run a Nema-17 motor with 100:1 gearing. The motor is rated for 1.7A. The power supply is set for 24V and 1.7A. However, I cannot get the driver to run the motor at its rated speed. It should be able to...

SJoha by Associate
  • 898 Views
  • 0 replies
  • 0 kudos

How to calibration fomula of CT for STPM34 ?

Hi All; I would like to calculate CT. I have formula below.I factor = VREF / (AI * CALIB_I * DPOW * KSI * KINT )   VREF = 1.18 from datasheet AI = 16 from datasheet CALIB_i = 0.875 from datasheet DPOW = removed KSI = Rshut = 0.05 ohm when I calcurat...

Gz by Senior
  • 809 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.