Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L7987L Not working as expected

Hello All,I am using L7987L to generate +15V from 24V. I have 10 same boards wherein I have used the same circuit (see below), I am able to generate 15V for 2 boards but in rest it is generating 1.22V only. R191 is 6.8kohm and diode D36 is US1M-E3/61...

Shivalee_0-1753767604520.png
Shivalee by Associate II
  • 331 Views
  • 1 replies
  • 0 kudos

Resolved! EVLVIPGAN50PD Modification for Standalone 12V Power Supply

Hi Sir, I would like to explore a specific use case that deviates from the standard design. My goal is to modify the EVLVIPGAN50PD to achieve a fixed 12V output, bypassing the USB PD negotiation functionality entirely. My intention is to utilize only...

TIENHUA by Associate III
  • 382 Views
  • 1 replies
  • 1 kudos

Mastergan5 - Switching losses

Hi,I'm interested in the Mastergan5 IC.To evaluate it for our use case in a Class-D amplifier we need information about switching losses.These are commonly provided by suppliers of half bridge ICs by providing the Eon and Eoff values over switching v...

Jannis by Associate
  • 269 Views
  • 0 replies
  • 0 kudos

Resolved! STM6600 Implementation Queries

Hi,We are implementing STM6600 push button controller for our design and we have below queries. Is there any pull up connected to PS hold pin, can I connect this directly to 3.3V logic MCU.For variant STM6600DU25DM6F, tON blank is 11.2s, Do we need t...

STPM32 triggers interrupt for non masked bits.

Hello,I use a STPM32 on a battery charge system. The STPM32 is associated with an ESP32 module.The driver used is from ST (V1.0, 17 may 2016).I want to detect some defaults with interrupt, and I configure the interrupt mask only for current and volta...

L9524C Control Input Signal Max. Duty Cycle Value

I have already using L9524C IC for glow plug controller. I have to must to learn that what is the maximum duty cycle value of Control Input (CI) PWM signal?And if I have apply continuous HIGH signal to Control Input pin, how L9524C works? Freq. is 40...

volkan1 by Associate
  • 297 Views
  • 0 replies
  • 0 kudos

L4985A_PFC issue

HiI am using L4985A for my 110W PFC design. During testing boost inductor current is getting distorted when i increase the load. And also, audible noise from the boost inductor. Here I attached the waveform. I used eDesign suite for designing and sim...

kanishka by Associate
  • 358 Views
  • 0 replies
  • 0 kudos

STC3115 - do we really need to use the RAM

HiI am looking into STC3115 for a device, powered by a LiPo battery. The battery is not removable, main CPU turns off during low-power states.Looking at the AN4324 system integration manual, it describes the procedure to use the embedded RAM to save ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.