Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Battery Analyzer

Dear sir,We want to design a Battery analyzer for automotive purpose. The range of battery voltage can be 9V to 36V. Can you please suggest me an appropriate part number or reference design.Regards,Manoj HiwarkarEmbedded Engineer,9916707384 / 8087764...

How to choose a proper MCU for DC fast charger ?

The interface between the Power Control Unit and the Control Unit is via CAN bus and the interface between the Communication Board and the Control Unit is via MQTT.Thank you for your time!

RLeit by Associate
  • 1063 Views
  • 0 replies
  • 1 kudos

BLDC motor speed control using PID

HI all,I am trying to implement PID algorithm to control speed of bldc motor. For that the RPM of the motor is measured using Hall sensor. Now I have to write the code for pid can anybody tell the logic or example!I have studied about the PID control...

svraj by Associate II
  • 1286 Views
  • 0 replies
  • 0 kudos

L5973D - 100% Duty Cycle Not Working

Hi,I have an L5973D set up for 28.5V output from 30V ish input for 2A current. The design requires the regulator to go to 100% duty cycle when the input voltage drops. At low currents (up to 1.5A) the device behaves correctly and smoothly transition...

JKing.3 by Associate II
  • 1070 Views
  • 0 replies
  • 0 kudos

power mosfet without body diode

Hello we need a power mosfet without body diode for bidirectional applications . Is there a power mosfet like above? as well as is there a mosfet that has substrate Pin available? Sincerely mohammad maghsoodi

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.