Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Stm32 Nucleo 767zi power on issue at 12V Vin.

Hi!I have an issue with stm32 Nucleo F767zi power setup.When I power up the stm32 Nucleo F767zi on 12V, the regulator ic and the controller chip heats up. Why?I have also changed the JP3 jumper to (Vin-5V) option. And the JP1 jumper is off.What's the...

HEMT and the new Powerflat 8x8 devices

After visiting the ST website the new GAN 700V Fet's got my attentionPart numbers starting with with SGT are under evaluation.Tested a few mastergan4, I found those very fast and could reach easy the 3 MHz with low rise and fall times (below 10ns)My ...

GentleRV by Associate
  • 316 Views
  • 0 replies
  • 0 kudos

Help with vnf1048f efuse

I have been trying to use the EV-VNF1048F with the vnf1048f high side switch on it to act as an SPI slave to an external ATSAME54 microcontroller master. I just want to read the current that the efuse experiances when connected between a DC power sup...

Resolved! The minimum system to program the STPMIC25APQR

Hi,We need to pre-program a large mount of STPMIC25APQR offline.So we would design a minimum system to program this device.My question is we only need to program this chip, which pins should be must. we would like to leave all other pins floated(not ...

Nluke.1 by Associate II
  • 460 Views
  • 2 replies
  • 0 kudos

EN 60730-1 and BTA41-800BRG

Hi All,We are making controller for 3 phase heater. It is ON/OFF controller, with heater in delta configuration with mains 400 VAC (phase to phase voltage).Heater is always connected to one phase, while other two are controller with ST's BTA41-800BRG...

Miso by Associate II
  • 820 Views
  • 4 replies
  • 0 kudos

VN9E30F Channel deatils

  VN9E30FTR – 6-channel high-side driver with 24-bit SPI interface Max. DC output current is internally limited to 35A for channels IOUT0, IOUT1, IOUT2, IOUT3, IOUT4, and IOUT5 Whether this 35A limit is shared across all channels or applies individu...

KumarTP by Associate III
  • 365 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.