Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

M0-7 vs 24V

Quote from page 11:The M0-7 standard high-side drivers are manufactured using STMicroelectronics® proprietary VIPower® technology. The devices are designed to drive 12 V automotive resistive as well as inductive and capacitive loads connected to grou...

FVan .1 by Associate III
  • 889 Views
  • 0 replies
  • 0 kudos

VNQ5050AK damages to short

I have a new design with VNQ5050AK. Controlled by an MCU via 2k2 resistors. 3 of channels are open, there is no load currently. One of channels has a small relay with a clamp diode. Supply voltage is 25V, I use laboratory supply with 2A limit, there ...

gylab by Associate
  • 805 Views
  • 0 replies
  • 0 kudos

STEVAL-ISB68WA is overheating on STEVAL-ISB045V1

I have the STEVAL-ISB68WA and STEVAL-ISB045V1 wireless charging development kits. When I place the receiver on the transmitter the power transfer is established, but within a few seconds the STWLC68 chip gets too hot to touch and the system shuts of...

JDupr.2 by Associate
  • 668 Views
  • 0 replies
  • 0 kudos

Resolved! Information about STDRIVE101

HelloIn one of the Webinars, ST mentioned, that a new Gate Driver STDRIVER101 should be available.I am working on an 48V BLDC drive (up to 60V) and I hope, this could be part of the solution.I can not find any information about this gate driver in th...

PBlat.1 by Associate
  • 1256 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.