Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-VP12201B

What is the possibility to feed the eSTEVAL-VP12201B from PFC with 385VDC?Do I still need to apply any filter at the DC input of the eSTEVAL-VP12201B when feeding it from PFC?In another word, I would like to feed it from a PFC with 385VDC without L1 ...

SShah.8 by Associate
  • 605 Views
  • 0 replies
  • 0 kudos

Supply management of powerstep01

I use powerstep01's datasheet "7.19 Supply management and internal voltage regulators".datasheet says: "VSREG must be always less than VBOOT". May be not Vboot, but Vbus?Also "The device can be protected from this event by adding an external low drop...

0693W0000059z3xQAA.png 0693W0000059z4HQAQ.png 0693W0000059z4qQAA.png

6 step with PTOOLS1V1 firmware with STEVAL-PTOOL1V1 board

I am working with the 6 step hall sensor firmware PTOOLS1V1. problem that i face isThis firmware is designed for 7 polepair and the motor with me is single polepair.i need to change the code to single polepair.plz any one help me to change code to 1 ...

ORaph.1 by Associate II
  • 3102 Views
  • 6 replies
  • 0 kudos

Viper Zero Dual Output Standby SMPS

HelloI am in the design/prototype stage of standby SMPS, specifications are belowInput range: 85VAC to 265VACOutput-1: 12V 0.150AOutput-2: 18V 0.150AOutput 1 will be the output on the secondary sideOutput 2 will be on the PRIMARY circuit side feeding...

SShah.8 by Associate
  • 648 Views
  • 0 replies
  • 0 kudos

STSPIN32F0 - Can I increase flash size?

I'm working with this MCU in a project and ran out of flash space. Would like to know if there is a wat to add an external flash to this or if there is bigger flash option.

DDomi.2 by Associate
  • 1045 Views
  • 1 replies
  • 0 kudos

Resolved! We are using STEVAL-SPIN3204 .While we testing the evaluation board,when we unplug the USB cable we are missing 12 volt @ VREG12,that is pin number 6 of STSPIN32F04B.

We are using STEVAL-SPIN3204 .While we testing the evaluation board,when we unplug the USB cable we are missing 12 volt @ VREG12,that is pin number 6 of STSPIN32F04B.Also the motor turned of.Also when we plug the USB cable 12 Volt coming back & Motor...

TGeor.1 by Associate II
  • 2543 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.