Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VNQ500 burns out

Hello, We are using the VNQ500 in our board to drive loads at 24V. While testing our board the VNQ500 causes troubles and we noticed high voltage going back to the inputs of the MCU. Our schematic is pretty simple: VCC, CE and EP are all connected to...

VXhur.1 by Associate
  • 818 Views
  • 1 replies
  • 0 kudos

VNH5050 diag pins and pwm input

I am designing a quad motor controller using 4 vnh5050. The motors will be controlled independently through INA1 - INA4 & INB1 and INB4 signals from uC.In order to keep pin count usage down:1) Can I connect the DIAGA and A DIAGB pins together and ...

FJB2069 by Senior
  • 885 Views
  • 1 replies
  • 0 kudos

VNQ500 Input High Voltage ambiguity

Hi,We will use VNQ500 in our circuit but I cannot be sure on Input high voltage value. In datasheet:Table 7 says Vih = 3.25 VoltsFigure 15 says Vih = 2.8 Volts and decreases with increasing temperatureWhich value should I take into account. Is it eno...

ASAHI.1 by Associate
  • 652 Views
  • 0 replies
  • 0 kudos

Resolved! Steval-esc002v1 bulk capacitors.

Hi what is the rationale to dimension the capacity of the to two bulk capacitors C22,C21?There are a lot of ESC COTS that havent these big caps.Thanks

FRagg.1 by Associate II
  • 1064 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.