Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STD25NF10T4 DPAK (TO-252) type A package outline

the part we received are slightly differ than data sheet for heat sink side. part# STD25NF10T4Just wondering if the same part has different subcontractors to make it ?Or they are made in different region since the STM labels also not common one

0693W00000BdRlpQAF.jpg 0693W00000BdRkrQAF.jpg 0693W00000BdRYsQAN.jpg
LYIM.1 by Associate
  • 768 Views
  • 0 replies
  • 0 kudos

Resolved! Lifecycle Data of ST L6219DS

I'm doing some research on stepper drivers an the L6219DS fits the exact needs. In order to do a proper evaluation i need to overview the lifecycle data. Can anyone provide this information for me. Would be a shame if this driver becomes obsolete ver...

SScho.3 by Associate
  • 1325 Views
  • 3 replies
  • 0 kudos

Resolved! Viper319XD does not hold the load

Hi All!I also used eDesignSuite to build two 3.3 and 15 volt power supplies. This is what the program generated for me:I made two boards according to these diagrams:In the process of testing them, I found that in the absence of a load, the voltage at...

0693W00000BbQmxQAF.png 0693W00000BbQn2QAF.png 0693W00000BbQnCQAV.png 0693W00000BbQnMQAV.png
VOsin.1 by Associate II
  • 2230 Views
  • 4 replies
  • 0 kudos

STEVAL-LLL009v1 Source Code

I purchased "STEVAL-LLL009v1" for the design of "LLC Resonant Conventor".I can download the HEX file from the following link, but I can't find the firmware source.Please help me.https://www.st.com/content/st_com/en/products/embedded-software/evaluati...

ykim.2 by Associate
  • 778 Views
  • 0 replies
  • 0 kudos

STEVAL-SPIN3202 Max current 15 Arms

Hello,1- can we use a higher current motor with the Dev -board since the Mosfets STD140N6F7 have Id 80A?2- in the schematic of the steval_spin3201 the VBUS and the VM are connected with JP2.My question is: if we supply VBUS with 48V and open JP2 can ...

what is 'H' mean in VN920B5HTR-E, no indication in datasheet

I am looking at the ST’s N-channel part VN920B5. But I notice there is VN920B5-E, VN920B5TR-E and VN920B5HTR-E. I look into the datasheet, it only shows VN920B5-E is tube, and VN920B5TR-E is tape&reel. There is no indication of what ‘H’ means for the...

RChen.5 by Associate
  • 826 Views
  • 0 replies
  • 0 kudos

X-NUCLEO-IHM03A1: link between the TVAL values of the Powerstep01 registers and the voltage across the shunt resistors ?

Hello everybody, I have a question I can't solve. I use the X-NUCLEO-IHM03A1. My question is : wath is the link between the TVAL values in the register of the Powerstep01 (see figure) and the voltage accross the shunt resistor of the board (100 m ohm...

0693W00000APL7SQAX.png
LHerm.1 by Associate III
  • 1895 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.