Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! L6470 and L6472 - What sets the speed of MOVE and GOTO operations? Using MAX_SPEED parameter imposes lower limit of 15.25 FS/sec and 15.25 FS/sec granularity.

I want to use MOVE and GOTO on some of the steppers at less than 15.25 FS/sec and with finer control than 15.25 FS/sec increments. Is there a way to specify MOVE and GOTO speeds other than by using the MAX_SPEED setting?

BMoul.1 by Associate
  • 1636 Views
  • 2 replies
  • 0 kudos

Resolved! What causes L6472 to power up / leave reset with bridges active?

I have designed a board with four seemingly identical motor drivers. The four L6472 are connected to an STM32-MCU via one SPI-interface, chipselect is handled by GPIO. They share a common reset signal, also GPIO. Because of the pull-downs on /STBY_RE...

harerod by Associate II
  • 4243 Views
  • 5 replies
  • 0 kudos

Gate driver for STY139N65M5

Hello,Has anyone used the 650V MOSFET STY139N65M5 in any of their designs? If, yes what was the operating frequency and the gate driver used in this case.Thanks,Mausamjeet

MKhat.2 by Associate
  • 1026 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.