2024-01-22 8:52 AM
2024-01-22 9:12 AM
What makes you think that Altium files should be available?
If you go to the Product Page for the board, schematics, etc, will be under 'CAD Resources'
2024-01-24 1:29 AM
The gerber files in CAD Resources is empty, so i think the layout and altium files can be available
2024-01-24 1:33 AM
You're assuming that ST use Altium.
Other systems are available ...
2024-01-24 2:21 AM
ok, How can i open the gerber files in CAD resources?
2024-01-24 2:29 AM
I can't see a Product Page for "steval-1sa170v1" - can you give a link?
2024-01-24 2:37 AM
2024-01-24 2:53 AM
Thanks.
So I see Gerbers, BoM, and Schematics all available for download there:
The Gerbers download as a Zip; the BoM and Schematics as PDFs:
Inside the Gerbers Zip:
2024-01-24 3:43 AM
i couldn't open the gerber files. so i asked for the layout or what is the method to open it?
2024-01-24 4:23 AM
Well, GERBER data is actually only intended for plotting a layout or producing a board, similar to PDF, which is also only intended for printing and not for re-layouting. However, you can use a GERBER viewer to orientate yourself on details from its data and derive your own layout. There are GERBER viewers that you can use for free, e.g. the one in the KiCAD package.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.