2022-09-28 8:26 AM
According to the datasheets for the L9963E and L9963, they state they are both "a Li-ion battery monitoring and protecting chip." There is no explicit mention that they won't work with LiFePO4 batteries and it's unclear if ST includes LiFePO4 batteries under "Li-ion" batteries. Want to confirm if LiFePO4 can be used with these chips.
Solved! Go to Solution.
2022-09-29 12:21 AM
Welcome, @Community member, to the community!
L9963 is already on NRND (Not Recommended for New Designs), new designs should use L9963E instead.
LiFePO4 has a minimum discharge voltage of 2.0V, a typical cell voltage of 3.2-3.3V and a maximum charge voltage of 3.60-3.65. L9963E covers a voltage range between 0.5-4.6V per cell, which therefore includes LiFePO4, but should also be designed for it by the software of the higher-level controller.
Does it answer your question?
Regards
/Peter
2022-09-29 12:21 AM
Welcome, @Community member, to the community!
L9963 is already on NRND (Not Recommended for New Designs), new designs should use L9963E instead.
LiFePO4 has a minimum discharge voltage of 2.0V, a typical cell voltage of 3.2-3.3V and a maximum charge voltage of 3.60-3.65. L9963E covers a voltage range between 0.5-4.6V per cell, which therefore includes LiFePO4, but should also be designed for it by the software of the higher-level controller.
Does it answer your question?
Regards
/Peter
2022-09-29 6:37 AM
Thank you for your answer @Peter BENSCH.
I figured you could use LiFePO4 with the L9963E.
Thank you for confirming this.
2022-09-29 7:10 AM
You're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.