2021-01-21 2:36 AM
There are two ways of BLDC motor solution. The one of solutions is EVSPIN32F0601S3 and the other is EVSPIN32F0601S1. I want to drive BLDC motor with sensor less. Which solution is match the goal? The motor specification is 100V D.C. 1A 100W.
Solved! Go to Solution.
2021-01-26 12:56 AM
Hello @TGoto.1 and welcome to the ST Community.
Both solution you mentioned are based on STSPIN32F0601 System-In-Package and fit your motor specification.
The main difference is in the shunt sensing topology:
You can choose the board according to the driving method (FOC or 6-step) and shunt topology (single or three).
Let me know if these info are useful to you, if yes please "Select as Best" button to close the topic.
2021-01-26 12:56 AM
Hello @TGoto.1 and welcome to the ST Community.
Both solution you mentioned are based on STSPIN32F0601 System-In-Package and fit your motor specification.
The main difference is in the shunt sensing topology:
You can choose the board according to the driving method (FOC or 6-step) and shunt topology (single or three).
Let me know if these info are useful to you, if yes please "Select as Best" button to close the topic.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.