2019-01-03 9:16 PM
Hi STM32,
I'm using STM32F401RE for communication with PC and want to send packet at 3-5 MBps speed.
I have to use MBED OS for deveopment kindly support for this also on my board 3x cryastal is not mounted only 2x so also want to conform my controller is running at 84Mhz or not.
Please help me on this.
Thanks & best regards.
2019-01-03 9:24 PM
The NUCLEO-F401RE does not have a USB connection directly to the target micro.
You'd need to add a high-speed PHY to get these types of speeds.
The F401 is provided with an 8 MHz clock from the F103 part performing the ST-LINK function.
If you want to test internal clocks, route to PA8 (MCO) and scope, or print out SystemCoreClock, etc.
2019-01-03 9:46 PM
Hi Clive,
Thanks for reply there was typo "3-5 Mbps" is the speed. SystemCoreClock show 84000000 value.
Which class can be used for "3-5 Mbps" usb speed. I wired out Pin PA_11 and PA_12 for USB connection and run HID example on F401RE, CDC crash after 8-10sec.
Thanks & Best regards
Chinkit
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.