2025-07-17 3:38 AM
Hello,
i'm starting a project with STM32F407VG and ADAU1466 DSP. The ADAU1466 generates the MCLK for the audio codec (ADAU1701), so far so good.
Now i'd like to implement full-duplex I2S communication between ADAU1466 and STM32 too using a different I2S port on the DSP. The idea is to set the STM32 as a slave receiver and let the DSP generate BCLK and LRCLK. In this context, do i need to provide master clock to STM32 too and if so, how? I mean, which pin should i use? For I2S2 i can see PC9 alternate function I2S_CKIN but i'm not sure if this is the proper way to provide external master clock.
Solved! Go to Solution.
2025-10-10 4:57 AM
Hello,
Yes you need to use I2S_CKIN when I2S in slave mode for STM32F407.
2025-10-10 4:57 AM
Hello,
Yes you need to use I2S_CKIN when I2S in slave mode for STM32F407.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.