2016-02-25 5:16 AM
Hello,
on my university we try to programm a STM32F072RB Dicovery Board with simulink embedded coder. But we've got some Problems. Every time we try to use the ADC-Block an error accure: ''Selected ADC has not been configured''. But it is configured in the cubeMX. Maybe someone has allready fix this issue. The CubeMX version is 4.13.0 The STM32F0 Lib. is version 1.5.0 Best regards T.I. #simulink-st32-mat-matlab-2015a #simulink-code-generate2016-02-25 11:48 PM
Hi Thomas,
ioc file including configured ADC must be selected from STM32_Config model. Then, ADC must be selected from ADC_Read block even if you have configured one ADC only. Please download STM32-MAT/TARGET V4.3.0, some modifications have been done regarding ADC. Best regards Pascal2016-02-26 5:57 AM
Hello mr Pascal,
that's exacly what I've tried. I drag the MCU Config block into the Simulink Model and selected the ioc file. But if I try to drag the ADC-Read block into the model the error appears. When I open the Blockmask I'am not able to select any channel of the ADC. I think the Problem is in the ioc file. In my created File for the STM32F072RB : #MicroXplorer Configuration settings - do not modify File.Version=6 KeepUserPlacement=true Mcu.Family=STM32F0 Mcu.IP0=ADC Mcu.IP1=NVIC Mcu.IP2=RCC Mcu.IP3=SYS Mcu.IPNb=4 Mcu.Name=STM32F072R(8-B)Tx Mcu.Package=LQFP64 Mcu.Pin0=PA0 Mcu.Pin1=VP_SYS_VS_Systick Mcu.PinsNb=2 Mcu.UserConstants= Mcu.UserName=STM32F072RBTx MxCube.Version=4.13.0 MxDb.Version=DB.4.0.130 NVIC.SysTick_IRQn=true\:0\:0\:false PA0.Locked=true PA0.Mode=IN0 PA0.Signal=ADC_IN0 PCC.Checker=false PCC.Line=STM32F0x2 PCC.MCU=STM32F072R(8-B)Tx ... There are only two lines which has informations of the ADC. In the ioc file of the examples for the STM32F407V (F4VGTx_OneADC.ioc) are much more configuration lines: #MicroXplorer Configuration settings - do not modify ADC1.Channel-5\#ChannelRegularConversion=ADC_CHANNEL_0 ADC1.ContinuousConvMode=ENABLE ADC1.DMAContinuousRequests=ENABLE ADC1.EOCSelection=EOC_SEQ_CONV ADC1.IPParameters=Channel5\#ChannelRegularConversion,EOCSelection,SamplingTe5\#ChannelRegularConversion,master,ContinuousConvMode,InjNumberOfConversion,Rank-5\#ChannelRegularConversion,ScanConvMode,DMAContinuousRequests ADC1.InjNumberOfConversion=0 ADC1.Rank-5\#ChannelRegularConversion=1 ADC1.SamplingTime-5\#ChannelRegularConversion=ADC_SAMPLETIME_3CYCLES ADC1.ScanConvMode=ENABLE ADC1.master=1 So maybe this can be the reason why the ADC-Read block can't read the configuration. I have also downloaded the newest version of the blockset as you say. But it is the same error. best regards Thomas Imdieke2016-10-04 11:41 PM
Hello Pascal,
I have downloaded the lattest version of STM32-mat V4.4.0.using Matlab 2015b 32 bit.
After all configuration steps done for ADC as you mentioned, I get the following error as:
''ADC s-function parameters list does not match the parameter list in the Mask''.
is it a problem with the compiled mex file or am I doing something wrong?
2016-10-05 2:47 AM
Hello
I think this is due to the configuration parameters and settingwithin MATLAB environment
. Have a look to themathworks site to have more info aboutconfiguration ofand
https://www.mathworks.com/help/simulink/slref/mask-parameters.html
. I recommend you to follow the displayed instructions inthe attached document ''STM32 MAT-TARGET HandsOn'' Regards ________________ Attachments : STM32_MAT-TARGET_HandsOn_v1_0.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htoq&d=%2Fa%2F0X0000000aXE%2F7DLPRJoilPm2pEkEG3gJk3EhO.syqLanQhorW4BAcr4&asPdf=false2018-06-12 4:30 AM
,
,
Hi,
Im experiencing the same problem only one port per ADC channel appears in the Simulink ADC block. I have found that its related to this line in the .ioc file:
ADCx.Channel-4\ ♯ ChannelRegularConversion=ADC_CHANNEL_x
There is only one such line per ,ADC channel even if multiple ports are selected, if I copy that line and change the port number it can now be read in Simulink. But this change is of course removed by Cube when project is saved.
Can you resolve this issue?
MathLab 2017b
STM32-MAT 4.4.2
STM32CubeMX 4.26.0
/Jonatan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.