2023-01-12 11:57 PM
Hi!
I am working with a STM32L053 MCU. I would like to write to the internal eeprom, and based on the datasheet it takes 3.2 ms.
I have doubts that during that time interrupts will be ignored. It is not clear for me why.
I thought that the code is in the flash and the eeprom is independent from the flash.
(Or maybe this EEPROM is not a real EEPROM, but emulated EEPROM in flash?)
Best regards
2023-01-13 5:57 AM
Hello @Attila Szabo (Community Member)
I can suggest the recommendation of AN4808 for STM32L0.
And firmware packege X-CUBE-NVMRWW.
https://www.st.com/en/embedded-software/x-cube-nvmrww.html
Best regards,
Romain,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.