2018-10-05 9:15 AM
Hi, I'm doing a hexapod with 18 servos and 6 legs (3 servos for each leg). I am using a core board and the Mbed environment with C language.
My question is: how could I initially consider the movements?
Initially I have declared all the necessary pins (18) and in which I have passed a pulse to servo number 1 to prove that the pin works on the board. I would like to know how to perform a simple movement even if they are 3 servos that would be 1 leg.
My code is the following:
#include "mbed.h"
#include "SoftPWM.h"
Serial serial(PC_6, PA_12);
SoftPWM servo1(PB_8);
SoftPWM servo2(PB_9);
SoftPWM servo3(PB_7);
SoftPWM servo4(PA_0);
SoftPWM servo5(PA_1);
SoftPWM servo6(PB_0);
SoftPWM servo7(PB_1);
SoftPWM servo8(PA_3);
SoftPWM servo9(PA_2);
SoftPWM servo10(PA_5);
SoftPWM servo11(PA_6);
SoftPWM servo12(PA_7);
SoftPWM servo13(PB_6);
SoftPWM servo14(PA_9);
SoftPWM servo15(PA_8);
SoftPWM servo16(PB_10);
SoftPWM servo17(PB_3);
SoftPWM servo18(PA_10);
int main() {
servo1.period_us(20000);
int servopulsewidth=1000;
int si_mueve = 1200;
int no_mueve = 1900;
bool movimiento = false;
servo1.pulsewidth_us(servopulsewidth);
while(1){
if (movimiento == true) {
servo1.pulsewidth_us(si_mueve);
serial.printf("YES: %f\r\n", servo1.read());
} else {
servo1.pulsewidth_us(no_mueve);
serial.printf("NO: %f\r\n", servo1.read());
}
movimiento = !movimiento;
wait_ms(250);
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.