2025-08-08 12:04 PM
Hi!
I'm working with the STM32F042K6T6TR (LQFP-32 package), and the documentation on mouser.com says that it is moisture sensitive. So what is the maximum temperature I can put this chip into the oven at (for ~24 hours) to dehydrate it. The working temp is max 85C, but I'm guessing it can take 100C when not powered, just dehydrating, right?
Link to datasheet
Thanks!
Solved! Go to Solution.
2025-08-08 12:14 PM
The max storage temperature range is 150 C. I wouldn't take it that high.
This seems to suggest 24 hr at 125 C.
2025-08-08 12:14 PM
The max storage temperature range is 150 C. I wouldn't take it that high.
This seems to suggest 24 hr at 125 C.
2025-08-08 12:16 PM
Thanks man, would've never found that. You're awesome!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.