2023-03-26 7:01 PM
I'm trying to implement "AN3969 EEPROM emulation in STM32F40x/STM32F41x microcontrollers" on STM32F407.
According to the documentation, "Interrupt servicing during program/erase is possible".
However, when actually installed, interrupts stop completely during the erase time.
What is the way around this?
2023-03-26 8:05 PM
It's an MCU not MPU, I fixed the tagging
If the ALL code / vectors / interrupts are all in RAM it might not stall. The erase or write of the Flash will block attempts to concurrently read from Flash.
2023-03-28 5:40 AM
Hello @UpStream,
Additionally, it is possible to relocate the interrupt vectors to a different bank of flash or some place in the user Flash memory that is not affected by the program/erase operation maybe temporarily to ensure uninterrupted interrupt service routine.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-29 1:11 AM
Thanks for the reply.
The EEPROM is using the default values sector 2 and sector 3.
The interrupt vector is also set to the initial value, sector 0. Is this a problem?
I am testing by porting "eeprom.c" to the sample code "TIM_TimeBase" using STM32F4DISCOVERY Discovery kit.
I moved most of the functions to RAM, but there is no improvement at all.
The move to RAM is
Edit STM32F407VGTx_FLASH.ld
----
_sidata = LOADADDR(.data);
.data :
{
. = ALIGN(8);
_sdata = .;
*(.data)
*(.data*)
*(.code_in_ram) <--- Insert
. = ALIGN(4);
_edata = .;
} >RAM AT> FLASH
----
Add to my code
----
__attribute__ ((long_call, section (".code_in_ram"))) void foo(void)
{
// Do something here
}
----
I used
Is there any help for me ?
2023-03-30 2:24 AM
Thank you always for your cooperation.
After that.
Interrupt vectors could also be switched to SRAM, but interrupts stop during Flash erase.
Am I still missing something?
// STM32F407VGTx_FLASH.ld //
/* Specify the memory areas */
MEMORY
{
RAM_BOOT (xrw) : ORIGIN = 0x20000000, LENGTH = 8K <--- Insert
RAM (xrw) : ORIGIN = 0x20002000, LENGTH = 120K
CCMRAM (xrw) : ORIGIN = 0x10000000, LENGTH = 64K
FLASH_BOOT (rx) : ORIGIN = 0x8000000,
LENGTH = 32k
EMULATED_EEPROM (rwx) : ORIGIN = ORIGIN(FLASH_BOOT) + LENGTH(FLASH_BOOT),
LENGTH = 32k
FLASH (rx) : ORIGIN = ORIGIN(EMULATED_EEPROM) + LENGTH(EMULATED_EEPROM),
LENGTH = 1024k - LENGTH(FLASH_BOOT) - LENGTH(EMULATED_EEPROM)
}
// system_stm32f4xx.c //
void SystemInit(void)
{
..........
/* Disable all interrupts */
RCC->CIR = 0x00000000;
memcpy((void*)0x20000000,(void const*)0x08000000,0x1FFF); <--- Insert
/* Configure the Vector Table location add offset address ------------------*/
#ifdef VECT_TAB_SRAM <-- Select define
SCB->VTOR = SRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */
#else
SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
#endif
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.