2019-07-23 6:45 PM
Hello, I' m working in team on a project using stm32 f100 series board. I should use an eeprom to storage and read some data, the eeprom is the following: CAT24C512WI-GT3 and I also have the init code for this I2C eeprom:
void io_ee_scl(char s)
{
if(s)
GPIOB->BSRR=GPIO_PIN_6;
else
GPIOB->BRR=GPIO_PIN_6;
}
void io_ee_sda(char s)
{
if(s)
GPIOB->BSRR=GPIO_PIN_7;
else
GPIOB->BRR=GPIO_PIN_7;
}
void io_ee_wp(char s)
{
if(s)
GPIOB->BSRR=GPIO_PIN_5;
else
GPIOB->BRR=GPIO_PIN_5;
}
char read_eeprom() //read eeprom function
{
return ( (GPIOB->IDR&GPIO_PIN_7) ? 1 : 0 );
}so I know the pins conected to my eeprom.
Considering I'm new in stm32 I need your help to understand how I can read and write datas on my eeprom....
Thank you
2019-07-23 7:35 PM
So you're bit-bang it and not using the I2C peripheral?
Here's the manual for your device http://www.onsemi.com/pub/Collateral/CAT24C512-D.PDF
It describes the signals on the I2C pins, and how the address (eeprom) and data are sent.
Perhaps you can extend your code to implement the functionality described?
2019-08-16 6:58 PM
Yes I am bit banging, can you suggest me where to find c code for do it?
2019-08-16 6:59 PM
Yes I am bit banging, can you suggest me where to find c code for do it?
2019-08-16 11:33 PM
I have shared in this forum an example of I2C bit banging with EEPROM simple customizable source code.
Now, use the forum to find it.
2019-08-17 8:48 AM
Do you mean this post: https://community.st.com/s/feed/0D50X0000AAI9JkSQL ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.