2019-05-03 4:45 AM
Hello,
I'm a beginner in the STM32 world so I bough the evaluation board presented in the step-by-step tutorial (from ST) the Nucleo Board with STM32L476RG, I followed the 5 steps and I was pretty sure to be able to download the example program and debug it. Unfortunately, after pressing Debug I've got this error: "Failure at line 13 in Target Software Startup Script. Please edit the debug configuration settings. Error finishing flash operation". I'm just guessing it could be due to a wrong memory bank selection but I dont know how to check it.
Any suggestion will be appreciate.
True studio version 9.3.0
2019-05-06 7:30 AM
Did you make any changes to the project? If you have an ST board you should be able to create a project for it and instantly debug.
I'm not familiar with this step-by-step tutorial, is it another project you import into TrueSTUDIO?
2019-05-06 12:54 PM
Hello Markus,
I've tried the example with non changes and I've also tried a new empty project created using Cubemx. I've got the same error, just on different lines but in both case the scrip command corresponding to the line error is "load".
2019-05-08 4:49 AM
I see. Could you enable the gdb server log in the "Debugger" tab of the debug configuration and paste it here? It's the little check box next to "Log to file:"
2019-05-08 1:42 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.