2019-07-10 1:34 PM
How can I debug a program that is being loaded and running from the QSPI external memory of the STM32F750 using the XiuP model?
2019-07-10 2:40 PM
Can't your tools do that now?
Do you need a debugger script to set up the memory interface properly? An external loader to support the memory on your board?
Sort of thing you're expected to do in Keil and IAR
2019-07-10 10:53 PM
I'm not sure I fully got you.
This is the case:
The XiP model provides a seamless load and debug experience similar to an internal Flash debugging. For
SW4STM32 IDE, the STM32CubeProgrammer should be used for application loading on external Flash
memories.
Given of all that, how can I perform this debug session?
2019-07-13 12:22 AM
Not sure what you mean precisely, but: You *build* the project with SW4STM32 and only program the image with STM32CubeProgrammer?! So actually it's build with gcc and debugged by gdb, that should be no problem as long as it's built with the appropriate debug symbols ("-g" should be sufficient). And even single-stepping through the parts in external memory should work "out of the box". Breakpoints are different though. In external merory you have to use 'hardware breakpoints', as gdb doesn't know how to erase/program the external memory (which would be required for 'software breakpoints').
hardware breakpoints: use address comparators inside the chip's debug interface, hence limited in number
software breakpoints: breakpoint instruction is placed into program code, requires reprogramming of program code
As I don't use SW4STM32, I can't tell you how to use hardware breakpoints by default there, you've to search the relevant docs.
2019-07-13 12:26 AM
Forgot to mention: probably it's sufficient to add a suitable option to one of gdb's init files (.gdbinit or similar), but where to place this file and other details I don't know.
2019-07-13 12:48 AM
Thank you Andreas for your answer.
The issue is that since I'm running my target project from the external QSPI flash in XiP mode I need to create a separated boot program that enable the QSPI and set it to memory mapped mode and then jump to the starting point of the main program in the QSPI (That was pre loaded to the QSPI by using the programmer)
The boot program is the one that is being loaded and running from the debugger and my question refer to how can I step\breakpoint the main program that is actually not loaded currently in the debugger.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.