2025-06-18 1:36 PM - last edited on 2025-06-18 1:49 PM by Andrew Neil
Dear Support Team,
I hope this message finds you well.
I am currently working on a project where I am trying to interface your BNO085 IMU module with an STM32L433RC-P Nucleo board. Despite numerous attempts, I have not been able to retrieve any meaningful data from the sensor.
Here are some of the key points of what I’ve tried so far:
I’m using I²C (also tested with UART) for communication.
Verified all hardware connections and logic level compatibility (3.3V).
Tried using both polling and interrupt-based approaches with STM32 HAL.
I have already tested the sensor separately with Arduino, and it works fine.
I also attempted different initialization sequences and delays, but the sensor remains unresponsive on STM32.
I would appreciate it if you could help guide me with any known compatibility issues or suggestions specific to using the BNO085 with STM32 microcontrollers. If you have any example code, documentation, or tips for STM32 integration, it would be immensely helpful.
Looking forward to your support.
2025-06-18 1:55 PM - edited 2025-06-18 2:03 PM
Welcome to the forum.
You need to give some more detail - please see: How to write your question to maximize your chances to find a solution.
Specifically:
@DUBEYISM wrote:your (sic?) BNO085 IMU module
The BNO085 isn't an ST product ?
https://www.ceva-ip.com/product/bno-9-axis-imu/ - have you looked there for software drivers?
2025-06-18 3:48 PM
Is the I2C address of the BNO085 shifted one bit left to use it with HAL? eg( bnodev.dev_addr=BNO085_I2C_ADDR1<<1; )
2025-06-19 12:52 AM - edited 2025-06-19 1:09 AM
@DUBEYISM wrote:I’m using I²C (also tested with UART) for communication..
If it supports UART, the best and easiest way to start is by connecting it to a terminal where you can send commands manually, and observe the responses - without all the complications and uncertainties of embedded firmware.
Then, once you've practiced and got familiar with what commands to send, and how the device responds, you'll be equipped to implement that in the STM32.
Similarly on the STM32, start by connecting it to a terminal where you can easily test that your code sends and receives data...
2025-06-24 10:08 PM
I am using adafruit bno085 breakout board and it is working fine when used with arduino it is working fine but when i am trying to use it with nucleo board its not working
2025-06-25 1:09 AM
@DUBEYISM wrote:I am using adafruit bno085 breakout board
You mean this: https://www.adafruit.com/product/4754 ?
Please always give a link to 3rd-party products - so that we can be sure what you're referring to.
Does it provide pull-ups?
Again, please show:
As @Vangelis Fortounas said, are you sure that you have the correct I2C address and that you are presenting it correctly?
@DUBEYISM wrote:it is working fine when used with arduino it is working fine
So compare & contrast your Arduino setup with your Nucleo setup.
The presentation of the I2C address is certainly a thing that could differ...
Put an oscilloscope on the I2C lines - are they clean & working ?
Put an analyser on the I2C bus - is the Nucleo sending the right stuff ?
Do you even get an ACK from the device?
You can check with HAL_I2C_IsDeviceReady
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.