2025-09-12 3:22 AM
Hi,
I am working on a project that needs Bluetooth support.
Our main MCU: STM32F411CE.
Bluetooth module: BlueNRG-2 (Brought a BLUENRG-M2SP module and then fabricated a simple custom breakout board)
Initially, I tried to use the official example project from STM32CubeIDE (Beacon, Central, and SensorDemoBLE). But it is not working. I could not discover any signal through a BLE scanner.
But I tried to read BLUENRG-M2SP directly using ST-Link and the RF Flasher utility. It worked.
I checked the SPI lines of the MCU using a logic analyzer, but I could not read any signal. Why does the MCU not send any data to the Bluetooth chip?
How do I set it as workable? Is there any simple example to power up this module?
2025-09-25 8:38 AM - edited 2025-09-25 8:38 AM
Hello @kaushika and welcome to the community;
Please make sure that the SPI lines (MOSI, MISO, SCK,.....) are correctly connected.
Could you please share the SPI configuration.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.