cancel
Showing results for 
Search instead for 
Did you mean: 

Would you confirm the STM8S207RBT3CRT can directly placed to the STM8S207RBT6C with no Hardware/firmware changes?

skim.1
Associate

We’re using STM8S207RBT6C for our current production. Due to the on-going IC shortage matter, we're trying to source a alternatives that can directly working on our existing design without any hardware nor firmware changes. We were able to find some batch of “STM8S207RBT3CRT�?.

We believe this higher temperature range product can be directly replace the current one without any Hardware and Firmware modifications. Would you please confirm this?

Thank you very much,

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Artur IWANICKI
ST Employee

I suppose you had in mind STM8S207RBT3CTR as replacement of STM8S207RBT6C. There are two differences between both. Temperature one (T3 means wider temperature range up to 125 degC instead of 85degC) and different final packaging (Tape and Reel instead of Tray / Tube). In such a case this new part can be used instead of previous one without any issue.

View solution in original post

1 REPLY 1
Artur IWANICKI
ST Employee

I suppose you had in mind STM8S207RBT3CTR as replacement of STM8S207RBT6C. There are two differences between both. Temperature one (T3 means wider temperature range up to 125 degC instead of 85degC) and different final packaging (Tape and Reel instead of Tray / Tube). In such a case this new part can be used instead of previous one without any issue.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.