2006-02-22 7:11 PM
Why my uart2 make program slowly?
2011-05-17 3:10 AM
My Uart2 initialize as following:
void Init_ComPort2() { EA=0; T2MOD=0; T2CON=0x30; TH2 =0xff;TL2 =0xDC; //T2 9600b/s 11.0592MHz RCAP2H=0xff;RCAP2L=0xDC; //T2 9600b/s 11.0592MHz ET2=0; //disable T2 interrupt TR2=0; SCON2 =0x50; PCON |=0x0c; //Used T2 IEA &=0xef; //Disable Uart2 interrupt TR2=1; EA=1; //CPU interrupt enabled } But,At main program ,when I use IEA |=0x10; //ES2=1 Enable Uart2 interrupt to Enable Uart2 interrupt, I find the all program run very slowly! The interrupt program as: void Com2Receive() interrupt 9 using 3 { unsigned char ch; if (SCON2& 0x01==0x01) //RI2=1 { ch=SBUF2; SCON2 &= 0xFE; //RI2 = 0; IEA &= 0xef; //ES2=0 switch(ch){ case 0xDD: ... break; case 0xDE: ... break; default: break; } IEA |=0x10; //ES2=1 } } And I find the interrupt program always run when I debug the main prigram. When I use Uart0 ,everything is oK!!! Why?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.