cancel
Showing results for 
Search instead for 
Did you mean: 

Why does the ST7FLITE09 EEPROM data lost? Emergency!!

jacktan1
Associate II
Posted on January 12, 2004 at 03:15

Why does the ST7FLITE09 EEPROM data lost? Emergency!!

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
jacktan1
Associate II
Posted on January 08, 2004 at 00:10

Hi,

My product which is using ST7FLITE09 as its control unit does not work well.

The product is Voltage Meter . After run a few days, all the EEPROM data lost. The Meter is embeded in Power Switcher. The environment of EMC is very bad.

I think maybe there are 2 reasons:

1. The program counter is modified by error, and the EEP write routine is excuted .

2. The EEP is erased by high electric shocks

But I am not sure about that.

who can help me.

Thank you for your help!

J.V.

jatin
Associate II
Posted on January 08, 2004 at 05:08

Could you clarify points below:

1. Are you verifying the data after writing it into the EEPROM? If not, you can verify it by reading it back so as to insure that the writing sequence is correct.

jacktan1
Associate II
Posted on January 11, 2004 at 04:43

I am sure it do the verify reading.

Thanks,

J.V.
jatin
Associate II
Posted on January 12, 2004 at 03:15

Could you give the part no. of the device and the environment conditions(EMC level, temp conditions etc)?

Have you tested the device in the normal environment (less noisy, normal temp.) ? If no, please test and provide the results.

Thanks.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.