2007-04-07 1:55 AM
What is the role of bit 9 in SCU_SCR0 ???
2011-05-17 12:40 AM
What is the role of bit 9 in SCU_SCR0 ?. According to the datasheet it is reserved, however in STR91x.S from Keil examples it is set to 1. Is there an errata or something about this?
SCU_SCR0_Val EQU 0x00000196 ; Setup System Configuration (and SRAM Size) IF SCR0_SETUP == 1 LDR R0, =SCU_BASE LDR R1, =SCU_SCR0_Val STR R1, [R0, #SCU_SCR0_OFS] ORR R1, #0x00000200 STR R1, [R0, #SCU_SCR0_OFS] ENDIF thanks, Andras2011-05-17 12:40 AM
hi Zouhair,
Thanks for your reply! Maybe you now something about WSR_AHB ? (AHB Wait state enable) http://mcu.st.com/mcu/modules.php?mop=modload&name=Splatt_Forums&file=viewtopic&topic=5147&forum=21 AndrasWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.