2003-10-29 2:45 AM
2003-10-13 4:39 AM
I use a ST72F264G2M6.
I am configured with option byte to use software watchdog. When i want to pass in wait mode (WFI instruction), i want to disable watchdog (bit WDGA=0, bit 7 of WDGCR) before activate WAIT mode and normally my watchdog don't wake-up the MCU. But my watchdog generate a reset and i leave the WAIT mode. I can't disable this watchdog, like if i was in case of Hardware Watchdog. There is someone to help me please !2003-10-13 4:54 AM
WDGA bit is cleared by default after reset. But if once set by the software can be cleared only by hardware after reset. So make sure that you have not set it after reset.
2003-10-27 1:40 AM
Thanks for your quick answer.
But my problem is that when i ma in wait mode, i have a reset by the watchdog which wake up my CPU. Is it normal or not ? For me, when i am in wait mode, i can to control the wake-up of my CPU, so the watchdog must not have an effect on the wake-up. Is this correct ? Your help is welcome !!!2003-10-29 2:45 AM
Wait mode has no effect on the watchdog. So it is normal if the CPU wakes up with the watchdog reset.
Watchdog is diasbled by default after reset. So, there is no chance for the watchdog reset unless it has been enabled after reset. But once it is enabled, it can be disabled only after reset. I hope it is clear. [ This message was edited by: Jatin on 29-10-2003 16:16 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.