2005-07-06 10:22 PM
2005-07-06 9:54 PM
Hi
According to the datasheet, the lowest stand-by voltage Vstby = 4.0V (without RTC and 32kHz oscillator). On the final version of ST10F276, could the Vstby be lower than 4V? Thanks2005-07-06 10:22 PM
Hi,
No the Vstby could not have a value lower than 4V. I think you ask this because you want to use a battery to back up the device in standby mode and that the batteries are usually 3.3V but unfortunatly this is not possible. Regards,We’re moving the ST Community to a new platform to give you a better and more reliable community experience.