cancel
Showing results for 
Search instead for 
Did you mean: 

VNLD5160

bestyeng
Associate II

Hi at all.
Can VNLD5160 work with a normal STM32 CPU with 3.3V logical levels?
I don't find this information in datasheet...
Thanks...

1 REPLY 1
Peter BENSCH
ST Employee

Well, the data sheet mentions two important points:

  • Vsupply = VIN = 4.5-5.5V

  • VINTH = 1...3.5V (table 8)

This means that you either use a level translator or configure the GPIO of the STM32 as an open drain with external pull-up. As the VNLD5160 can only switch at a few kHz, the simpler and cheaper open drain variant may be sufficient.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.