2021-06-07 1:42 PM
The datasheet does not explicitly call out maximum current that can be monitored with the "current_sense" pins but it appears to be 1.5A. Does that imply that this is also maximum continuous per output current that the part is rated to? Or is it 3.8A - the minimum short circuit current? Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.