2003-06-19 1:29 AM
2011-05-17 2:54 AM
Hello,
We are trying to implement a debug system of the code for upsd323x . In that we have mapped boot flash as code & primary flash as data in a combined space mode. How should set the initial value of the VM register using the PSDsoft express? I don't find the option in the PSD menu configuration. Thanks in advance for any comments. Regards, Jokin2011-05-17 2:54 AM
Hi,
The initial VM setting is derived from the Define MCU/DSP and PSD section Step 3 - Select PSD configuration The lower two pulldown options select where the Main and Secondary flash should be , DATA, PROGRAM or BOTH To select memory addressing, this follows the pin definition page. Once the pin definitions are defined, click Next>> This will take you through page definition and addressing (Chip Select Equations) Please see for a full guided version of PSDexpress regards, Simon [ This message was edited by: sjh on 12-11-2003 16:22 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.