2005-01-11 10:49 AM
2004-05-11 2:10 AM
Hi,
I'm using an STPC Consumer with a TFT 1024x768 LCD connected to the on board VGA. I'm using the VGA BIOS from Elpin System. The problem was that work at a frequency of 63Hz instead a frequency of 60Hz. I'm not familiar with the VGA register, can you help me to focus on the register intrested on frequency adjust and screen centering thanks2005-01-11 10:49 AM
Do you have a VGA register set example for a 1024x768 display ?
Perhaps in a 32kBios, even with 63 Hz. Best Regards FlipflopWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.