2005-11-29 2:47 AM
2005-08-25 10:37 PM
I am trying to implement the standaard function printf to put a string to the uart of my STR710 uC.
I already can send/receive an character array via uart, but I like to improve my send/receive function to be able to send via printf. But how do I configure the send function so that it sends the printf string via the UART? Regards, Jimmey2005-11-28 10:41 PM
Hello ibtiss,
iam using the GNU toolchain, i inculded all the files u mentioned, but i still need the makefile and the linker script, these two are really confusing me. iam new to that field would anyone please upload a generic form of these two? Regards,2005-11-29 2:47 AM
Hello zouhair,
iam using gnu gcc v.3.4.3 for arm-elf, with newlib, ill be very appreciated if u can help.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.