2006-08-08 3:39 AM
2006-08-07 10:22 PM
Hi.
I want to reset USB port without unplugging and re-plugging cable. I tried to setting FRES and PDWN bits in USB_CNTR register. I also tried to PowerOff() function in usb_pwr.c but they are not working. How can I make the PC re-recognize my USB STR711 device? Thanks yusuf2006-08-07 11:03 PM
Hi Jozef,
To generate an USB reset from device point of view you have to disconnect and re-connect the pull-up resistor (on the D+ line). You have to provide a schematic to disconnect this resistor using a GPIO pin. Please find attached a simple example of schematic able to connect and disconnect the pull-up resistor using one GPIO, two transistors and three resistors. Regards, AnisAs :D ________________ Attachments : USB_reset.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtPS&d=%2Fa%2F0X0000000aPb%2FpjMKRLzxLvsHrUpPyWagUYfxL3uRU.sMdyIYh06wT_U&asPdf=false2006-08-08 3:39 AM
Hi AnisAs,
Thank you for your urgent reply. It's working!!! regards yusufWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.