2004-08-25 12:08 AM
2004-08-24 11:46 PM
I have problem with USB device detection and data corruption on the STPC Atlasis board.
Does any one get this problem? How to get the Atlas USB working correclty? Thx.2004-08-25 12:08 AM
Yes, this problem is resolved and it was an impedance mismatch on the board. This is the workaround.
Add two capacitors to ground (100pF) on USB D- line after the ESD device USBDF01. The USB was tested with different devices under Wince4.2 & Win98 and it works correctly.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.