2005-10-03 8:17 PM
2005-10-03 5:30 AM
Hi
I've compiled the AN1797 example and tried it on the evaluation board. This works fine. The board echo back all characterers send from Hyperterminal. I then program the same example into our own target board. But the baudrate seems to wrong. Our target board uses a 4MHz crystal, but the UART_Config function uses the RCCU_FrequencyValue to calculate the baudrate on runtime. So the crystal frequency should not be the problem or is it?2005-10-03 5:42 AM
Double check your 71x_conf.h header for a proper definition of RCCU_Main_Osc. This is necessary for the Library to calculate a proper baud value. You should see something like...
/* Main Oscillator Frequency value = 4 Mhz */ #define RCCU_Main_Osc 4000000 Best regards, Ryan.2005-10-03 6:03 AM
thx...
I had to remove ''extern const u32 RCCU_Main_Osc;'' from the RCCU.h file to be able to compile. - But it didn't work. Same symptoms as before.2005-10-03 7:27 AM
Sounds like you are using the Anglia SARM Toolchain whicj uses a differant method than the standard libs. If so the definition for the RCCU_Main_Osc is at the top of your startup file - should be startup.s by deafult.
Regards sjo2005-10-03 8:17 PM
Yes, Im using the Anglia SARM Toolchain. I've found the constant in the startup.s file. And now it works!
@ SJO - Thank you very much for your help!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.