2006-06-06 1:27 AM
2006-06-06 1:27 AM
Hi, I am having some trouble with UARTs. It happens not very often, but it happens.
I am using the 4 UARTs. In the middle of a data transfer through UART3, (half duplex, which sends some data, waits ACK, sends more data, and so on..) it suddenly hangs my application. By making some debug with JTAG, I noticed that UART0 enters in the interrupt routine countinously (as if some interrupt bit is always set), but I dont know why. These are the values of some registers I got from UART0: CR: 0x05A9 IER: 0x0140 SR: 0x0006 My communication module (the one who handles the 4 UARTs) is using interrupts and FIFOs. It just makes some buffering of data. This code is the ISR:Code:
static void CommISRHandler(commbuffer_t *pBuffer, UART_TypeDef *UARTx) { uint16_t FlagStatus; uint16_t nError; FlagStatus = UART_FlagStatus(UARTx) & UARTx->IER; /* Check any TX Interrupt */ if (FlagStatus & (UART_TxEmpty | UART_TxHalfEmpty)) { do { /* Is there any data to send? */ if (0 == pBuffer->BufferTxCtr) { /* No, so turn off TX interrupts */ UART_ItConfig(UARTx, UART_TxEmpty | UART_TxHalfEmpty, DISABLE); break; } /* Put new data */ UARTx->TxBUFR = CommGetCharISR(pBuffer, &nError); /* Repeat until UART is full */ } while (UART_FlagStatus(UARTx) & UART_TxFull); } /* Check any RX Interrupt */ if (FlagStatus & (UART_RxHalfFull | UART_TimeOutNotEmpty)) { do { /* Add Data to Buffer */ CommPutCharISR(pBuffer, UARTx->RxBUFR); /* UART_RxBufFull in fact means UART_RxBufNotEmpty */ /* So, repeat until no data is present */ } while (UART_FlagStatus(UARTx) & UART_RxBufFull); } } The ISR has two parameters: commbuffer_t *pBuffer -> points to the corresponding buffer structure UART_TypeDef *UARTx -> points to corresponding UART My 4 UART Interrupt handlers only call this routine, for instance:Code:
void Comm0ISR(void) { CommISRHandler(Buffers[0], UART0); return; } Any suggestion? Regards,We’re moving the ST Community to a new platform to give you a better and more reliable community experience.