2004-02-10 2:09 AM
2011-05-17 2:58 AM
Hello all,
I‘m using uPSD3334DV in my card and the platform has 2 serial ports. I initiated a communication between UART0 and a PC serial port, and it’s working good. I tried to use UART1 for another channel but the serial signal don’t appears. In the debugger the program jump to UART1 interrupt every byte transmit. My program for initialize UART0 and UART1 : Ea =0 //---------- UART0 ------------- timer2_baud = (65536L - ( (FREQ_OSC * 125L) / (4L * 19200L))); RCAP2L = (timer2_baud & 0x00FF); // Timer 2 Reload low byte RCAP2H = (timer2_baud >> 8,); // Timer 2 Reload high byte T2CON = 0x34; // Set RCLK = 1 ,TCLK= 1 Timer2 select for uart0 // TR2 = 1 start Timer2. P3SFS|=0x03; // Configure P3.0,P3.1 as UART0 pins SCON = 0x40; //uart0 - mode 1 - SM1= 1 SM0 = 0 // 8 BIT variable data rate RI = FALSE; // prepare to receive REN = 1; // receiver enable - register ES = 1; // Enable Uart0 interrupt //---------- UART1 ------------- TMOD |= 0x20; // Timer 1 mode - 8 bit auto reload SCON1 = 0xE0; // SM1= 1 SM0 = 1 mode 3 - 11 bits data TH1 = 0xfd; // 19200 baud - must change recording to OSC PCON |= 0x4C ; // set RCLK1 = 1 , TCLK1 = 1 - recive and // transmit CLK enable // smod1 =1 UART1 - boud rate *2 TR1 = 1; // baud rate generator run ! RI1 = FALSE; // prepare to receive REN1 = 1; // receiver enable - TCON register P1SFS0 |=0x06; // Configure P1.2,P1.3 as UART1 pins IEA |= 0x10 ; // ES1=1 Enable Uart1 interrupt The problem is why the serial signal don’t appears. hanan [ This message was edited by: hanan54 on 04-02-2004 10:11 ]2011-05-17 2:58 AM
Please try the following settings:
PCON |= 0xCC; P1SFS0 |=0x0C; Also, please see Table 42 (SCON0 and SCON1 Register Details) on page 48 of uPSD33XX datasheet, SCON1 = 0xE0; (i.e. SM1= 1 SM0 = 1 mode 3 - 11 bits data)2011-05-17 2:58 AM
Thanks Upsd,
I change my program according to the last post and It help to solve the problem. Thank you, Hanan2011-05-17 2:58 AM
Hanan
Can you post a complete working example of the UARTs? DOWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.