cancel
Showing results for 
Search instead for 
Did you mean: 

Tinybios+usb+cdrom

balaji_softproff
Associate II
Posted on October 14, 2006 at 07:42

Tinybios+usb+cdrom

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
balaji_softproff
Associate II
Posted on October 04, 2006 at 05:26

hello,

We use atlas evaluvation board. We used tiny bios and able to boot slackware from harddisk. Does anyone know how to add boot from cd in tiny bios and also what changes for USB support in tinybios.

Tried gs bios usb working but in tinybios it is not working (Probably irq table not set in tinybios)

thanks in advance

Balaji

kaouther
Associate II
Posted on October 09, 2006 at 12:17

Hello,

The validated Bios working on Eval board are the one published on intranet. From where did you got the tiny bios? Did you receievedd this bios with another eval board?

balaji_softproff
Associate II
Posted on October 14, 2006 at 07:42

Hi,

I got the bios from TinyBios website. The ''readme.txt'' notes in it says CDROM boot support not available in it we should add it ourself.

So if you have the source code of tiny bios which supports CDROM boot as a request from me, can you provide me so I could look into it and try to implement it in the code I have.

I hope you reply me with a positive answer

thanks

Balaji

[ This message was edited by: balsara on 14-10-2006 11:22 ]

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.