2022-01-11 3:25 PM
Solved! Go to Solution.
2022-01-15 10:58 AM
Hi,
ARR value should be one less than the desired value. In your case instead of 250 use 249.
TIM4_TimeBaseInit(TIM4_PRESCALER_64, 249);
2022-01-11 4:01 PM
I accidentally posted it blank.
I'm using TIM4 to develop a prototype product application, and the interval between interrupt events is about 0.4%.
With the minimum required implementation as shown below, the interrupt event occurrence interval was 1.004 ms (The ideal is just 1 ms).
For a 15 minute timer, there will be a large gap of +3.6 seconds.
INTERRUPT_HANDLER(TIM4_UPD_OVF_IRQHandler, 23)
{
GPIO_WriteReverse(GPIOD, GPIO_PIN_5);
TIM4_ClearITPendingBit(TIM4_IT_UPDATE);
}
void main(void)
{
CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSE, DISABLE, CLK_CURRENTCLOCKSTATE_ENABLE);
GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_OUT_PP_LOW_FAST);
TIM4_DeInit();
TIM4_TimeBaseInit(TIM4_PRESCALER_64, 250);
TIM4_ITConfig(TIM4_IT_UPDATE, ENABLE);
TIM4_Cmd(ENABLE);
enableInterrupts();
while (1)
{
}
}The MCU is STM8S003F3U6TR.
I am using a 16MHz external oscillator with a deviation of ± 30ppm.
What causes this gap? Can software handle it?
Regards,
Gotoda
2022-01-15 10:58 AM
Hi,
ARR value should be one less than the desired value. In your case instead of 250 use 249.
TIM4_TimeBaseInit(TIM4_PRESCALER_64, 249);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.