2005-08-08 9:39 PM
2005-07-11 3:39 AM
hi everybody,
I'm developing firmware for a ST72F324J6 (42pin sdip package) microcontroller. I want to generate a pwm waveform with timer A and applied it to pin OCMP1_A (pin 13). attached you'll find the C code I wrote down. just for test purposes the duty cycle is approx 50%. the code do not produce the expected result: no pwm appear on OCMP1_A pin. I checked several times the few line of code i posted here but i'm not able to find the bug in them.... pehaps some missing sttings... I followed step by step what I found on the ST72F324 manual.... I think my error is naive but I can't find it! macro I used for setting and resetting bits (_bset & _bres) are tested and functioning. any suggestion ?? thanks a lot for your precious help regards ________________ Attachments : timerA.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzuq&d=%2Fa%2F0X0000000bTi%2FeCXQDSOKlvA93faDFwjM9TVmh8tvRPzTIzGi8.F7.wE&asPdf=false2005-08-08 9:39 PM
It is difficult to suggest something from your attached code. The best way is to use the ST7 software libarary containing the 16-bit timer peripheral. It can be downloaded from the same site.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.